9/25/2006 12:19 PM | |
Joined: 4/24/2006 Last visit: 8/8/2024 Posts: 8713 Rating: (1166) |
Hello, An USB-RS232 convertor will not work Take a look at the following Thread: /tf/WW/en/Posts/4312 Best regards, Wizard |
10/20/2006 5:59 PM | |
Posts: 1 Rating: (0) |
[:)] Yes, i do it whit 3 different adaptor USB->RS232, you must chose COM 1 as number of the USB port. It is in system hardware manager, under COM/LPT... |
10/20/2007 7:30 AM | |
Posts: 158 Rating: (3) |
hey guys, i think i have foung a solution for the S5 with usb dilema. I had the same problem as well and i made some changes in the parameters and comp port settings and i managed to go online with the PLC through USB. I have attached the steps on hw to do it. Hope it will help solve the S5 with USB dilema.. Ragards. Attachment5 Simple Steps to Configure Serial to USB conversion on St….pdf (3401 Downloads) |
This contribution was helpful to3 thankful Users |
4/4/2009 10:34 AM | |
Posts: 1 Rating: (0) |
THX for the information it's useful, but cannot download |
9/17/2011 6:33 AM | |
Posts: 4 Rating: (0) |
your Attachment not available any more. Can you send me mister?? thank... Best Regard.. |
Follow us on