10/21/2018 2:33 PM | |
Joined: 12/18/2014 Last visit: 8/8/2024 Posts: 33513 Rating: (4163) |
Hello 820T, try this. AttachmentSTEP5_Print.zip (285 Downloads) |
This contribution was helpful to1 thankful Users |
10/21/2018 4:18 PM | |
Joined: 12/18/2014 Last visit: 8/8/2024 Posts: 33513 Rating: (4163) |
And STEP5 is so old, so I have not worked with it for years. Do you have the manual for Step5 V7.2? |
10/21/2018 6:16 PM | |
Posts: 51 Rating: (0) |
You Sir are a HERO :) I will go to the workshop and try to do just that - thank you so much . . . .a few minutes later . . .I hope these are the correct files :) Its actually a 'RAR' file but I've renamed it ZIP to be able to upload it Attachment820T.zip (235 Downloads) |
Last edited by: 820T at: 10/21/2018 6:44:43 PM |
|
10/22/2018 11:06 AM | |
Posts: 51 Rating: (0) |
Thank you, but I have managed to fathom it out and produced a .PDF - the attached is just the main program block PB202 Next task is to annotate it with labels for the inputs and outputs that I know from the circuit diagram. AttachmentPB202.pdf (224 Downloads) |
Follow us on