1/2/2008 10:02 AM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hi Genelec, When you open old project, please save and compile. Are you having any errors? Perhaps you can perform an OS update, see link: http://support.automation.siemens.com/WW/view/en/19701610 Best regards, Wizard |
1/2/2008 1:21 PM | ||
Joined: 5/8/2006 Last visit: 10/16/2024 Posts: 1085 Rating:
|
Hi,
do you have the right settings in ProTool and on the OP170B? OP170B: You should look into the Transfer Settings of the OP170B. Is the serial port enabled? Link for the manual of the OP170B: (page 3-9) http://support.automation.siemens.com/WW/view/en/1838350 ProTool: Transfer Settings of ProTool: "Datei > Download > Preferences...". Is the serial port selected? Cable: Works yourserial cablecorrect? Maybe you should change your cable. Bye |
|
1/2/2008 3:17 PM | |
Posts: 22 Rating:
|
Hi Zak1 Yes, all setting is OK, most likely cable, I am working it out Best regards Genelec |
1/2/2008 5:51 PM | |
Posts: 22 Rating:
|
Hi! The cable is ok, but problem is still present Best regards |
1/3/2008 9:03 AM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hi Genelec, Well, you should deinstall the CP5511 in Device manager of Windows. Then start PC without CP5511. Please reboot PC but now with CP5511 it will automatically be recognized and installed. Also have a look at the following faq's: http://support.automation.siemens.com/WW/view/en/9853739 http://support.automation.siemens.com/WW/view/en/12259435 http://support.automation.siemens.com/WW/view/en/19279714 Hope it will help. Best regards, Wizard |
1/3/2008 2:20 PM | |
Posts: 22 Rating:
|
Hi Wizard1 just after, thanks also for the links, I have downloaded this programm. Best regards Genelec |
1/3/2008 6:55 PM | |
Posts: 22 Rating:
|
Hi Wizard! Here you are a file in zip. And perhaps I could backup with Prosave this software from an identical working OP and try to download to new one, but I fear that a cure my be worse as desease File is sent divided in three parts. Thanks for help Best regards Genelec AttachmentTDOP.zip (497 Downloads) |
1/3/2008 6:58 PM | |
Posts: 22 Rating:
|
Part_2
Attachmentsdb.zip (472 Downloads) |
1/3/2008 7:29 PM | |
Posts: 22 Rating:
|
Hi Wizard! I am trying to send this project in part, but some problem occured with uploading with Part 3, due this I had to divide into 4 parts Best regards Genelec AttachmentPart_4.zip (467 Downloads) |
1/3/2008 7:50 PM | |
Posts: 22 Rating:
|
eventually I got uploaded
AttachmentPart_3_.zip (482 Downloads) |
1/8/2008 5:42 PM | |
Posts: 22 Rating:
|
Hellp Wizard! Today I have tried to transfer project over MPI, but without success, but there is a link:http://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=19109408&caller=view and it states follows: PC/MPI-Adapter and USB/MPI-Adapter are not released for transfer. Best regards Genelec |
1/11/2008 9:30 AM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hello Genelec, The PC-adapter has nothing to do with CP5512 It's strange you still cann't transfer to Panel. Please have a look at following link: http://support.automation.siemens.com/WW/view/en/13032411 Perhaps it's useful Best regards, Wizard |
1/24/2008 7:58 AM | |
Posts: 22 Rating:
|
Hi Calafalas Sorry for delay, just emerged simultaneosly bulk problems in anothere areas and so far Touch Panel runs OK, but still no access over MPI, as attachment you find diagnostic windows of PG/PC as well Accessible Nodes - in the next posting, perhaps you can give me same idea to get the staff further connected over MPI. Best regards Genelec AttachmentDiagnostic.zip (596 Downloads) |
1/24/2008 8:31 AM | |
Posts: 22 Rating:
|
Hi Pictures with Accessible Nodes Regards Genelec AttachmentAccessibleNodes.zip (595 Downloads) |
Follow us on