5/15/2023 9:55 AM | |
Joined: 1/30/2020 Last visit: 8/7/2024 Posts: 16 Rating:
|
So what do i need to do now. As CPU is not going on run mode. |
5/15/2023 10:20 AM | |
Joined: 12/18/2014 Last visit: 8/8/2024 Posts: 33511 Rating:
|
If you have the program please then upload it as a ZIP file. |
5/15/2023 2:10 PM | |
Joined: 1/30/2020 Last visit: 8/7/2024 Posts: 16 Rating:
|
Hi, Attached is the program. I believe its the IP 246 (positioner card) that is causing problems. But I am not able to download the IP246 program as well. When i try to download it says "watchdog error". Attachment734.zip (445 Downloads) |
5/15/2023 2:29 PM | |
Joined: 1/30/2020 Last visit: 8/7/2024 Posts: 16 Rating:
|
Attached is the program. I believe its the IP 246 (positioner card) that is causing problems. But I am not able to download the IP246 program as well. When i try to download it says "watchdog error". Attachment734.zip (487 Downloads) |
Follow us on