1/25/2023 8:14 PM | |
Joined: 2/17/2020 Last visit: 5/27/2024 Posts: 28 Rating: (0) |
another attachment |
1/27/2023 9:31 AM | |
Joined: 10/16/2007 Last visit: 2/23/2024 Posts: 627 Rating: (45) |
Hallo, the next panel you can use/transform to is the MP370/MP377 and then switch KTP1500. Maybe check here (hopefully also available in English). Regards Scott |
1/30/2023 2:53 PM | |
Joined: 8/3/2009 Last visit: 5/27/2024 Posts: 12984 Rating: (1654) |
Hello GonzagaCassio you have to migrate to WinCC flexible 2008 Sp2 or older then you can change device and migrate to TIA Portal also. Here are some manuals for these two steps:
Bye Murof |
Last edited by: Murof at: 01/30/2023 14:54:08If this Information really helps, you could use the Rate function |
|
Follow us on