8/28/2024 9:21 PM | |
Joined: 8/12/2022 Last visit: 10/14/2024 Posts: 1 Rating: (0) |
Hello guys, I hope you are having a good day. I have a problem, I want to read a DB of data from my S7-1200 plc from a Modbus TCP/IP client, I have made all the configurations and it reads the data correctly up to byte 120, if I want to read above this byte I get a error "Illegal Data Adress", So I would like to know if there is a limit of bytes per DB to expose them in an MB_SERVER or is there something I am overlooking, or is there another way to achieve this. I am attaching a zipped file of photos of my configurations. Thank you!
AttachmentConfig.zip (115 Downloads) |
Follow us on