10/28/2021 9:52 AM | |
Joined: 10/28/2021 Last visit: 3/23/2022 Posts: 1 Rating: (0) |
How to reset the password in s7 1200 1214c DCDCRLY ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 10/28/2021 13:01:44New subject after splitting |
|
11/1/2022 7:42 AM | |
Joined: 3/11/2019 Last visit: 5/29/2024 Posts: 1450 Rating: (263) |
Hi, the card 6ES7954-8LE03-0AA0 is correct. But the card must be empty, and as addition, the card must be configured as "Transfer" Card, as mentioned in FAQ above, otherwhise it will not work. You can also have a look at this chapter in the manual, in my opinion it is described well. SIMATIC S7 S7-1200 Programmable controller-> delete existing data es mentioned in the manual, but do not delete hidden files -> configure the card as Transfer Card, as mentoined in the manual (up to/including step 4.) -> use the empte transfer card, as mentioned at the end of the chapter regards sancruz |
Feedback appreciated, please rate |
|
Follow us on