(0)| 5/23/2025 6:45 PM | |
|
Joined: 3/14/2008 Last visit: 1/22/2026 Posts: 2233 Rating:
|
Hi, You can do this without any problem, but when you compile the program with "Generate module drivers", the interconnections for the driver blocks are automatically set visible again. So, basically it is not of any use... |
|
If I could help you, you can use the RATE button. Thank you. |
|
| 5/24/2025 7:18 AM | |
|
Joined: 3/14/2008 Last visit: 1/22/2026 Posts: 2233 Rating:
|
Hi, If you insert a new driver block, make the interconnection invisible, assign a symbol and compile the AS, then the driver connections are made visible again after compile. If the connections are already created, you can hide them and the do not appear. It is only for new driver connections. The color coding is a solution, make sure other people know about this |
|
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on