3/2/2018 11:11 AM | |
Joined: 4/28/2015 Last visit: 6/3/2024 Posts: 3345 Rating: (377)
|
Hi, I've found two websites - Rancher and Resin.io (docker based). Have a look at these two solutions, maybe one of them suits your requirements! Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to1 thankful Users |
3/5/2018 8:18 AM | |
Joined: 4/28/2015 Last visit: 4/21/2024 Posts: 578 Rating: (43) |
When using Docker as deployment format, you just need to recall that standard images, even if they seem to run fine, tend to lack the build workaround for the Quark processor on the IOT2000. Last time I checked, that included the images resin.io was suggesting for that processor. The result can be sporadic crashes in the field. So you need to rebuild all images from source, eg. using the meta-iot2000 layer. This thread may also give some useful hints: https://support.industry.siemens.com/tf/ww/en/posts/update-by-usb/185892/?page=0&pageSize=10 |
This contribution was helpful to2 thankful Users |