10/15/2015 10:16 AM | |||||||||||||
Posts: 153 Rating: (7) |
I am posting this post today cause I am recieving so many confusion by my friends related to expert list.I am every time saying same thing but they do not remember. I think this is the better way to describe in forum. Everybody knows there is 4 tab in the expert list look how it works 1st TAB-User-defined Parameter List You can create your own list of IMP parameters.you can copy the parameter from main expert list or you can directly enter,copy from external source also possible.you can make multiple list ,can delete and can make with comment line.can add as a watch table,can save as list, as value list,and as a executable scripts Description As of Version 4.0, you can create user-defined parameter lists. A user-defined parameter list contains a subset of the optional parameters from an expert list. Only the parameter name and the comment are saved in the user-defined parameter list. The parameter value is stored in the associated expert list for the associated drive device or DO. When parameter values are changed, the value in the expert list is also changed automatically. In the user-defined parameter list, you add the most important parameters and assign them a comment or heading, e.g. structuring of parameter groups. Parameters can also occur several times or in unsorted order within a user-defined parameter list. User-defined parameter lists depend on the context in which they are opened because they always refer to the expert list that is opened in parallel. Thus, if a parameter list is created for Drive1 and opened in the context of Drive2, certain parameters may not be present there or have a different version. In this case, information text will be displayed in the user-defined parameter list.
The user-defined parameter list is stored as ASCII text in the *.cdl format. User-defined lists that were created with the versions V3.2 or V3.2 SP1 can be opened in V4.0. The associated stored values are ignored. The parameter list is saved automatically as *.cdl by default. User-defined parameter lists that were created with V4.0 or later can no longer be used in an older version. As of V4.2, you can also create a user-defined list as a watch table Create/open user-defined parameter list:
2nd TAB this tab is used for already saved user difined expert list. these values list will be default saved in the s7 project under U7 and cdl data but u can save on your own location. these parameter list values will be same as set value in online/offline project 3rd TAB-User-defined value list this tab is basically used for already saved user defined values or main expert list values. the difference from 2nd tab is these values will give the comparison of online offline value in the project from the last saved values these values list will be default saved in the s7 project under U7 and cdl data but u can save on your own location Description
As with user-defined parameter lists, user-defined value lists contain a subset of the freely selectable parameters from an expert list. The value and the unit are stored for each parameter contained therein. In this way, parameter settings can be saved for a specific time and restored later or transferred to another device. The following can be set:
Open Value List Dialog Box
A comparison with the current values of the DO will be made in the value list dialog when a user-defined value list is opened. The contents of the value list serve as reference for the comparison. Any parameters contained in the value list that are not present in the current object will be marked as NOT AVAILABLE with an orange background in the second column (similar to the comparison dialog). If the object is ONLINE, the comparison is made with the online values; if the object is OFFLINE, the comparison is made with the offline values. The values of the current object (namely, the second column) can be edited directly in the value list dialog, analog to the comparison dialog. The color assignment will be changed immediately after exiting the edit field. The values in the first column cannot be edited. 4th TAb Used for saving the valueformat ,list format or scripts format. Converting user-defined lists into watch tables You have created user-defined parameter or value lists in an older SIMOTION SCOUT version. You can still open these as usual from the expert list, but they are converted automatically into watch tables. A reconversion is not possible, but the same functions are available in the watch tables as in the user-defined lists.
Procedure for creating a watch table
Save expert list as script Description As of Version V4.0, you can save a parameter set as a chain of write/read requests in script form within the expert list. The script will be saved in the script folder below the object. If the script folder does not exist, it will be created. You can use this functionality, for example, to save the result of a comparison with the factory setting in script form or to perform a series commissioning of a number of drives by taking the parameterization from a reference drive. Script example ' 10/1/2006 from "Script_test.cdl" converted script APP.LogActive = TRUE ' Activate output "Readable parameter Value = (Parameters(2, 0)) ' Drive operating status "Writable parameter Parameters(5, 0) = 2 ' BOP operating status selection Restrictions and special features To permit the script also to be executed successfully online, certain unlocking mechanisms are required. For all MICROMASTER drives (MM4xx, ET200, G110, G120), during the conversion, start and stop sequences will be prefixed to the visible parameter set. To improve the understanding, a comment is automatically added to the required inserted sequences. The inserted sequences are:
Unlocking mechanisms are not yet supported for SINAMICS drives V4.0. If the parameters are read-only because of the parameter values of the CU (e.g. p9, p10, p301, p922, etc.), an error message for each will be output in the Scripting output window. Parameters that change the structure (e.g. p140 for the SINAMICS drive) are not treated differently. When the script is created, you must take into consideration that these parameters are at the top of the selected parameter set. Any changed unit systems will not be used when the script is executed. When the script is executed you must ensure that the transfer of the parameter values is sensible in the current context. Any locks in the expert list (e.g. dependent of the access level, motor code, p340, etc.) are not used. A write request is added to the script for all green and blue (write) parameters. To create an executable script:
Mukesh Soni |
||||||||||||
10/15/2015 11:15 AM | |
Posts: 153 Rating: (7) |
Yes Mr. ChristophD sorry for that. Should I remove that |
12/11/2018 10:55 PM | |
Posts: 1 Rating: (0) |
How would I convert an expert list to a Db in S7? What does the "Convert list to S7 Db" do? |