6/13/2021 1:08 PM | |
Joined: 9/28/2008 Last visit: 8/8/2024 Posts: 14 Rating:
|
Hi Georg, Yes the communication it´s ok. I can see all parameters Voltages, Currents, Alarms, etc, from my PG and from WinCC advanced, the backup battery works perfect when a main supply switch off happens. All modules are originals from Siemens I´ve bought 6 units two or three weeks ago. It´s the first time than I´m working with softplc CPU 1505SP, but at the moment I see all very similar to other 1500 cpu. The firmware version used in 1505SP is V21.8. In the attached file you can see the control cabinet and the configuration hardware on TIA for UPS. I´ve checked all firmware version and exact reference model for all modules. Thanks for your help. Litos97 AttachmentUPS1600_CONFIG.zip (471 Downloads) |
Follow us on