3/16/2015 12:27 PM | |
Joined: 7/2/2010 Last visit: 5/9/2025 Posts: 53 Rating:
|
Hello ! In a simovert masterdrive type 6SE7138-6NJ62-3BA0 we replaced motor by new one. The new motor power is bigger and also rpm are higher. I need to know how to fill the new motor data and if i can use another motor data set and make the inverter to work with this new data set without deleting the old motor data set. I also need help on some calculation or method for parameters like motor reactance or stator resistance. Also maybe it needs to change other parameters which are related with motor protection values. Attached are the old motor nameplate, new motor and also complete inverter parameter set. Attachmentnew motor.pdf (1151 Downloads) |
3/16/2015 12:30 PM | |
Joined: 7/2/2010 Last visit: 5/9/2025 Posts: 53 Rating:
|
old motor data
Attachmentold motor.pdf (809 Downloads) |
3/16/2015 12:31 PM | |
Joined: 7/2/2010 Last visit: 5/9/2025 Posts: 53 Rating:
|
complete drive parameters
Attachmentklin head fan 2006-7-3.rar (936 Downloads) |
3/16/2015 12:32 PM | |
Joined: 7/2/2010 Last visit: 5/9/2025 Posts: 53 Rating:
|
i tried also to fill a service request but when i reached at the end "send" button does not work |
9/13/2022 9:04 AM | |
Joined: 8/24/2016 Last visit: 4/22/2025 Posts: 18 Rating:
|
thanks for your support |
Follow us on