5/24/2023 6:55 AM | |
Joined: 4/13/2023 Last visit: 6/9/2025 Posts: 5 Rating:
|
Good Afternoon all, I want to use ET-200SP,IM-155-6DP ( 6ES7155-6BU01-0CN0) module. Which consists of 3 DI modules, 3 DO modules, 6 AI modules and 2 AO modules. Please tell me is there any requirement of PM module in configuration? If yes then how many ? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/24/2023 09:28:45New subject after splitting |
|
5/24/2023 4:27 PM | |
Joined: 5/6/2010 Last visit: 9/12/2025 Posts: 2031 Rating:
|
Hello, the ET200SP DI, DO, AI, AO will supplied via the base unit. There are "basicly" 2 types, a light grey and a dark grey version (also more than 2 types). The light grey base unit will connect to the 24 V and open a new potential group for the modules at the right side. One of the easiest way to select the right base unit and built potential groups for your ET200SP is the Also you can find the description of the base unit and so much more at the SIMATIC ET 200SP Manual Collection Hope this is helpful. |
Follow us on