Industry Online Support
Technical Forum
7/3/2023 8:44 AM | |
Joined: 3/31/2023 Last visit: 6/18/2024 Posts: 25 Rating:
|
I am reading data from Siemens PLC via OPCUA to node-red using OPCUA client node. Things were working fine for about 1/2Hr. But after some time i got an error in node red debug window."" [31m Client node error on: error: [" error at active reading: Transaction has timed out ( timeout = 15000 ms , request =Read Request)"] [39m"" What is this error and how do i mitigate this error (I have attached the screenshot).???? If someone already asked and answered this question here, please refer me to that question. Also, I'm reading data(not subscribing) using OPCUA client node in node-red
AttachmentFiles.zip (638 Downloads) |
Last edited by: Jen_Moderator at: 07/03/2023 11:20:10Flow added as .txt file. All files added as .zip file. |
|
Follow us on