6/16/2021 7:16 PM | |
Joined: 6/10/2021 Last visit: 9/6/2022 Posts: 2 Rating:
|
I have a problem and hope you can help me. I'm trying to upload as a new station a safety et200 CPU 1510SP F-1 PN but I can´t. The error says: Online upload is not supported. The consistent fail-safe upload is not enabled for the online device. Either the online device doesn't support fail-safe upload or the appropriate setting in the safety administration editor is not active and downloaded. Can you help? what shlould I do to upload the project if i don't have the offline project?
------------------------------------------------------------------------------------------ |
Last edited by: CS Moderator at: 06/17/2021 10:27:09New subject after splitting |
|
6/29/2021 11:38 AM | |
Joined: 2/17/2020 Last visit: 9/11/2025 Posts: 1251 Rating:
|
Hi JJimenez13, I'm afraid that, as you will be able to see in the following link, the option 'Enable consistent upload from the F-CPU' had to be checked when the first download was made, so you will not be able to upload as a new station from the F-CPU: "The" Upload from device (software) "or" Upload device as new station (hardware and software) "function is only possible for S7-1500 F-CPUs if the" Enable consistent upload from the F-CPU "option is activated for the F-CPU in the Safety Administration Editor and the project data is loaded to the F-CPU afterwards. ". Loading project data from an F-CPU to a programming device / PC I hope this information is useful to you. |
A rating will be well appreciated. |
|
Follow us on