10/15/2024 9:08 AM | |
Joined: 7/19/2022 Last visit: 9/11/2025 Posts: 436 Rating:
|
Hello AutoGen_5717228, The fault F30005 means that there is an overload in the application. In these cases, it is necessary to first check the wiring of the motor terminal box to ensure that it is at 230V or 400V, then check and if there are any doubts, restart the motor using the TIA Portal Startdrive wizard, entering all the motor data correctly and finally run the Motor ID (p1900 = 2) of the motor. If after doing all this the fault continues to appear, it will be necessary to use the Startdrive diagnostic tool called "Trace" and graph current consumption (r68), speed (r21) and temperature (r25). |
If this Information really helps, you could use the Rate function |
|
10/16/2024 11:52 AM | |
Joined: 10/11/2006 Last visit: 9/8/2025 Posts: 6039 Rating:
|
Hello AutoGen_5717228, |
With best regards, |
|
Follow us on