10/14/2024 7:20 PM | |
Joined: 9/21/2012 Last visit: 9/3/2025 Posts: 4695 Rating:
|
You need a clean memory card for the PLC also. |
10/22/2024 6:32 AM | |
Joined: 3/11/2019 Last visit: 9/1/2025 Posts: 1653 Rating:
|
Hi, as Hati already mentioned, you ned a clean (empty!) MMC. So my question is, ist it a new unused MMC, or just another MMC which was also used previously? Nevertheless. Just delete the data on any of the MMCs. Afterworks it should work with both of them. Do NOT format with windows! regards sancruz In STEP 7 (TIA Portal), how do you format an MMC or MC and why does a message appear saying that the SDB 7 is not loaded?Which devices can you use to read from, write to or delete from an S7-300 MMC (Micro Memory Card) outside the CPU?How do you delete the data on an MMC (micro memory card)?How do you format or reset an MMC (Micro Memory Card) for SIMATIC S7-300 CPUs? |
Feedback appreciated, please rate |
|
10/22/2024 6:32 PM | |
Joined: 1/5/2021 Last visit: 3/15/2025 Posts: 15 Rating:
|
Hello, Tonight I've tried to perform the total reset of the old mmc. I still need the password for this when I try to do this. I did some more tests as well. When the old mmc is inserted there is no problem and I can easily connect to the cpu. Is there an explanation for this? Doet the new one need to be formatted? Please note that the new card actually is a new card which is empty! I'm looking forward to hearing from you! Kind regards, Jobbbooo AttachmentDifference between cards.pdf (282 Downloads) |
Follow us on