10/31/2024 11:33 AM | |
Joined: 8/3/2009 Last visit: 9/17/2025 Posts: 16442 Rating:
|
Hello The KTP600 Basic is a Basic Panel 1st Generation that has only a newest available Image Version of V12.X.X.X. Since V14 Siemens has changed PLC Sim communication. Check also this FAQ: https://support.industry.siemens.com/cs/de/en/view/109742764 -> So you cannot use a newer FW on the Panel (there is no newer!) So a communication from KTP600 Simulation and PLC Sim V14 or newer is not possible. With real HW it works. Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on