10/31/2024 11:51 PM | |
Joined: 10/8/2020 Last visit: 9/3/2025 Posts: 1 Rating:
|
I am looking for a way to install an MTConnect agent on an IoT 2050 with the following characteristics: 6ES7 647-0BA00-1YA2 Operating System: Linux iot2050-debian 5.10.104-cip3 Firmware version: V1.3.1 Installed image: IOT2050_Example_Image_V1.3.1 So the main problem is that you have to read data from a Fanun CNC with a native Focas protocol, but that machine already has an MTConnect adapter installed. Image 1. Therefore, I need to have an MTConnect Agent on IoT2050 to process the data, and have HTTP and XML. Then process the data in node red. Image 2. HTTP Request: Make the request to the MTConnect adapter to obtain the data. XML: Converts the XML response to JSON. Function (Extract Variables): Extracts variables based on the provided XPath paths. What recommendations could you give me to be able to make an MTConnect agent? Is it possible to do it on an IoT2050? Is there a manual or application example of MTconnect and IoT2050? AttachmentImages_MT_Connect.zip (149 Downloads) |
Last edited by: Moderator_Lan at: 11/04/2024 07:59:26Text formatting optimized |
|
Follow us on