11/6/2024 6:21 AM | |
Joined: 5/12/2006 Last visit: 9/15/2025 Posts: 22710 Rating:
|
for each version a own VM |
11/6/2024 3:04 PM | |
Joined: 5/6/2022 Last visit: 9/15/2025 Posts: 589 Rating:
|
Hi Itlj, The problem with installing different versions is that only one database can be installed in the same environment. I mean, for example, two different versions of Unified-Unified, Professional-Unified, Professional-Professional or a version of WinCC Classic cannot coexist in the same environment. All these versions have a database and this will lead to problems. Therefore, you can install WinCC Advanced versions on the same virtual machine, as these do not have a database with a Unified version in your case, but you cannot install further Unified versions in the same environment. To install more Unified versions, you have to create virtual machines. I hope I have been able to explain myself clearly. Best regards!
|
If this Information really helps, you could use the Rate function |
|
Follow us on