2/28/2025 6:58 PM | |
Joined: 2/28/2025 Last visit: 3/4/2025 Posts: 2 Rating:
|
I have WinCC v. 7.5.0.0 running on Windows Server 2012. I have read through the following: How do you set up Autostart for WinCC? How do you avoid synchronization problems with the Autostart of WinCC Runtime V7? lunch the wincc RT without using the "autostart" option I don't have a "CCStartStop.exe" executable (apparently that comes with SP2). There is no AutoStartWinCCRT value in the Registry, but there is an AutoStartWinCC key with multiple values (Activate, ProjectName, StartInServiceMode, etc.). Regardless, I used the cited materials to put together a batch file with the AutoStartRT.exe command (see below). As described, I set the AutoStart configuration to to have "Autostart active" deselected and "Activate project at startup" is selected. The project is in service mode under a local user account. Task Scheduler was set up to run the batch file on computer startup after a delay. Batch command: AutoStartRT.exe C:\HMI_DX\DX.mcp /Activ:yes /LANG=ENU /EnableBreak:no When I start the computer, I can see that the Task Scheduler ran the batch file and that AutoStartRT.exe was running. However, the WinCC project did not start (no windows, no error dialogs, no change to the sharkfin in the Windows tray) after running for 30 minutes. I killed the AutoStartRT.exe process. Then I ran the same command from the command prompt. That resulted in an error message of "AutoStart is not possible". If I just set the AutoStart configuration with "Autostart active" selected (no Task Scheduler or batch file), the project starts fine when the computer starts. Any suggestions on what else I might need to do to successfully start the WinCC project from a batch file/command prompt? -Chris |
3/7/2025 10:40 AM | |
Joined: 8/3/2009 Last visit: 9/19/2025 Posts: 16461 Rating:
|
Hello U_15e5b524-3a35-4... Why do you use WInCC V7.5 without any SP or Upd? I would highly recommend using the latest SP or also at least the latest Update. A lot of issues regarding performance, stability and security have beed fixed in the Upd/SP. WinServer 2012 is also with V7.5 SP2 released: https://support.industry.siemens.com/cs/de/en/view/64847781 Bye Murof |
Last edited by: Murof at: 03/07/2025 10:41:24If this Information really helps, you could use the Rate function |
|
Follow us on