3/9/2025 10:05 AM | |
Joined: 5/26/2011 Last visit: 9/16/2025 Posts: 483 Rating:
|
Here is a photo of whole tag management page. |
3/12/2025 12:26 PM | |
Joined: 8/3/2009 Last visit: 9/18/2025 Posts: 16447 Rating:
|
Hello G_R_E_Y_31 there are several ways of creating Tags over the OMS+ Channel. have a look at this FAQ: https://support.industry.siemens.com/cs/de/en/view/101908495 I would recommend using the SCADA Export Tool or connecting online to the PLC and select the needed tags. An absolute addressing should only be used in special configuration and also you would need non optimized DBs (which you will not want to be used in S71500) Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on