3/11/2025 1:11 PM | |
Joined: 5/6/2022 Last visit: 9/9/2025 Posts: 589 Rating:
|
Hi ManZan, From my experience, all variables that are configured as cyclic and with a low time (<=1s), will be recorded in the fast data log. Everything else goes to "slow data log". This is discussed in the TIA Portal manual: In the "Result" section at the bottom you will find the following: "All logging tags to which these settings apply are logged in the Fast data log. All logging tags to which these settings do not apply are logged in the Slow data log." I hope I was able to help you!
|
If this Information really helps, you could use the Rate function |
|
3/13/2025 3:47 PM | |
Joined: 12/2/2014 Last visit: 3/13/2025 Posts: 14 Rating:
|
Ok, thanks! |
Follow us on