(0)| 6/3/2025 7:35 AM | |
|
Joined: 9/7/2023 Last visit: 12/21/2025 Posts: 2 Rating:
|
Hello, I have a problem with the Chiron FZ12 machine (ncu571.2_mmc100.2). After I loaded the machine's nc and plc data (the data in the floppy is the same as the machine's serial number), the machine has no system alarms. When I press the power on button, it says infeed ready,only have axis reference alarms. The LED status on the NCU is normal. There are two problems. 1- The MMC does not connect automatically. The counter on the monitor starts counting until we press the ^ button and then enter address 6. The hmi boots. 2- The MCP all LEDs blink. The MCP address is set to (dip switch) 7 . I cannot open ob100 in the PLC program to see its contents. The MCP address in DB7 is 6. I set the MCP address to 6, but the mmc does not boot anymore. How can I open ob100? Can anyone help me? Thanks AttachmentFz12ncu571.2mmc100.2.zip (165 Downloads) |
Last edited by: @AutoGen_1013265 at: 06/03/2025 07:36:38Last edited by: @AutoGen_1013265 at: 06/03/2025 07:39:12Last edited by: @AutoGen_1013265 at: 06/03/2025 08:37:37Last edited by: @AutoGen_1013265 at: 06/06/2025 22:17:10A |
|
| 6/6/2025 10:17 PM | |
|
Joined: 9/7/2023 Last visit: 12/21/2025 Posts: 2 Rating:
|
Can anyone help me |
Follow us on