7/1/2025 11:25 AM | |
Joined: 12/18/2014 Last visit: 9/3/2025 Posts: 35914 Rating:
|
Hardware Support Packages for “ET 200SP e-Starter”Attached are the latest Support Packages for ET 200SP e-Starters for different TIA Portal versions ready for downloading. These Support Packages will permit you to configure e-Starter modules that are not contained in the hardware catalog of your TIA Portal installation. TIA Portal V19
TIA Portal V20
Note Pay attention to the software requirements specified for each Support Package (for example, for STEP 7 Professional V19 this means that at least STEP 7 Professional V19 or a higher Service Pack of version V19 must be installed). Sample Installation of HSP in the TIA Portal
Result After successful installation, the “Detailed information” dialog shows the “HSP0441 ET200SP e-STARTER 1.0” as installed. |
This contribution was helpful to
1 thankful Users |
Follow us on