3/21/2022 10:27 AM | |
Joined: 8/3/2009 Last visit: 9/5/2025 Posts: 16343 Rating:
|
Hello crazyCow I think you have to use already: https://support.industry.siemens.com/cs/de/en/view/109798498 If you use a new FW in PLC and WinCC >=V7.5.2.4 then you have to use the way in the FAQ. Do you use a Windows Server Operating System? (You need one, because of the big amount of connections). And do you also use a SIMATIC NEt Softnet license for up to 64 connections? Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
8/4/2025 8:55 PM | |
Joined: 2/15/2022 Last visit: 9/3/2025 Posts: 1 Rating:
|
Hello, have you solved this problem? I have also encountered a similar problem and would like to ask for advice. |
Follow us on