9/11/2025 6:54 AM | |
Joined: 8/3/2009 Last visit: 9/11/2025 Posts: 16400 Rating:
|
Hello elnur_sucayev first of all, do you want to use a faceplate with the tag prefix (so something like THIS) or do you want to use screen windows with tag prefix and without the use of a "faceplate"? its because the way of doing this solutions is a bit different But this requirement should be possible. for example the tag dynamization for the trend control and the filter for the alarm control you can set in a script in the loading event of the screen. you can use the prefix information in the script for example in VBS with the "parent" to read out the tag prefix property from the screen window. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on