(0)| 8/26/2009 12:26 PM | |
|
Joined: 10/8/2008 Last visit: 7/2/2025 Posts: 43 Rating:
|
Hello all, We made a communcation see programm and my last tread, some weeks ago. The PLC is the server and the client is a module from IPS (foxboro). In our project there are 7 ID build up, when communication is set up for the 7 ID's i can see that the: ID 1 makes roughly 12 comms / sec. with the client ID2 makes roughly 10 comms / sec. with the client ID3 makes roughly8 comms / sec. with the client .. ID7 makes roughly2 comms / sec. with the client When comms is setup for all off the ID's, there is no error,after 5 minutes the comms with ID 7 is lost, and not buildup again. the module FB102 is not given an error ? Is it possible the slow down, or control the comms from ID 1, 2, etc. This tooimprove the comms of ID 7. Thanks in advance Jan Landewers. AttachmentTcp.zip (846 Downloads) |
Follow us on