(0)| 9/13/2010 1:28 AM | |
|
Joined: 9/27/2006 Last visit: 1/14/2026 Posts: 12480 Rating:
|
Hello lam; The Sicomp IMC01 is a computer that runs a special OS, RMOS3, I believe. It is also quite old... the following manuals are from 1999. https://support.automation.siemens.com/WW/llisapi.dll?func=ll&objaction=csopen&objid=10805713&nodeid0=10805713&idx0=S&nav0=tree&lang=en&siteid=cseus&aktprim=0&extranet=standard&viewreg=WW As to whether you can upload the files from the Sicomp to a PG, that will depend on whether the OS is compatible with Windows, what type of files you want to transfer and what you want to do with them eventually. If you have some specific questions about such a legacy system, please start a Support Request (before you start another rant!). Hope this helps, Daniel Chartier |
Follow us on