6/1/2011 3:53 AM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating:
|
Hello, .MCP is WinCC File Format and .hmi is WinCC Flexible file Format. I am not sure for the coversion of WinCC Project to WinCC Flexible. Dear All, Is there any Conversion available fro WinCC to WinCC Flexible? Splitted from FILE TYPE CONVERSION. |
Last edited by: O_Moderator at: 6/3/2011 10:57 AMnew subject after splitting VANDE MATARAM..... |
|
6/1/2011 6:41 AM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hello, But you could migrate WinCC to WinCC Flex. http://support.automation.siemens.com/WW/view/en/18796902 ( page 25 - Migrating WinCC projects ) you can see what will receive after migrating.The result is nearly nothing. Better start from the begining and create new project in WinCC Flex. I think this is the right way. Best regards, Hristo Mihalev |
This contribution was helpful to
4 thankful Users |
Follow us on