1/4/2007 9:33 AM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hello tudong, You can use a DP/DP Coupler. To exchange data between the two Profibus masters. Here is a link to manual: http://support.automation.siemens.com/WW/view/en/1179382 Best regards, Wizard |
1/4/2007 11:02 AM | |
Joined: 9/27/2005 Last visit: 8/29/2025 Posts: 203 Rating:
|
Hallo, maybe this Link, which shows a Master-Slave-Communication between two PLCs, will be helpful. http://support.automation.siemens.com/WW/view/en/19449428 Greetings Morten |
1/4/2007 10:02 PM | |
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
[quote user="tudong"]I'm a new memeber. I have 2 CPU 315-2DP, each of them has an ET200M. Now i want to connect them via Profibus. Please tell me the solution in this case Hi Tudong, Welcome on this forum. [:)] Under the next link you have the possibilitys to communicate for MPI and Profibus DP What are the options for exchanging data between CPUs via MPI/PROFIBUS DP For a complete list of all possible communication with SIMATIC you may look also to the FAQ Communication with SIMATIC S7 I hope that you may find all the answers off your questions [8)] |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on