4/4/2007 3:41 PM | |
Posts: 18 Rating:
|
Good Morning,
I've added a ET-200S IM151-1 Standard remote rack to an existing profibus network. Everything is configured correctly, all cabling, hardware, etc has been checked and rechecked. After downloading error free hardware configuration to the CPU via ethernet routing, the newly added module, address 57, never is recognized.
I've also problems with changing modules in the ET-200S IM-151, order#: 6ES7-151-1AA0*-0AB0. These were OEM added modules and will NOT accept any changes to their hardware configuration. I've tried using different .GSD files, etc. to no avail.
I've attached the hardware export to this message. I'd appreciate any input to my problem.
Thanks
Attachmenta2_entangler.zip (1048 Downloads) |
Follow us on