Industry Online Support
Technical Forum
2/7/2014 1:45 PM | |
Posts: 391 Rating: (50)
|
SINUMERIK 810/820, GA3, Installation Guide http://support.automation.siemens.com/WW/view/en/21898397 6.2.2 MODE switching SET UP OVERALL RESET: In this MODE the machine cannot be operated. The following functions are available: • Overall reset (cancel function) • Load standard MD (input function) • RS232C (V.24) activation • PLC cannot be started via PG • Read in/out PLC programs with S-5 operating system or C/PM operating system (%PCP)• Read in/out PLC alarm texts (% PCA)6–4 © Siemens AG 1990 All Rights Reserved 6ZB5 410-0DL02SINUMERIK 810 |
Follow us on