1/22/2008 2:54 PM | |
Posts: 10 Rating:
|
Hi Late, i'm using the y-link for non-redundunt Dp devices and for my distributed I/Os that are away fromthe master (PLC), as u can see in the attached file(ET200M.JPG) the I/Os in the Ylink network are many and to make them redundunt would cost more than one YLink, So i had to use Ylinks for some I/O racks. my only problem is with the Channel Driver Blocks, when i use "Generate Module Drivers" the I/Os that are not from PCS7_V61 profile in HWConfig are not generated (Check the attachedLOG file attached "Grinding_Module driver" ) and so the channel driver block does not get the MODE input !!! and the block gives "BAD Quality". the Ylink only accepts ET200M from the Additional Field Devices which are not from the PCS7_V61 profile. is there a solution for this??? AttachmentET200M.zip (702 Downloads) |
Follow us on