2/1/2006 5:05 PM | |
Joined: 9/23/2005 Last visit: 9/10/2025 Posts: 4416 Rating:
|
Hi, With MPI/DP interfaces you can reach 1000m in 187,5 Kbits without repeater (MPI/DP interfaces are isolated). With MPI or PPI interfaces you can reach only 50m (MPI or PPI interfaces aren't isolated). However the maximal distance is also a function of the bauld rate. With just one paar repeater you can reach 1000m in 187.5 kbits (sufficient for your application). With 12Mbits the maximal distance is 100m. You can access a table in the specification of the repeater (IK PI 2005 catalogue page 5/47 – www.siemens.com/simatic/printmaterial ).You can use his TS Adapter without problem. |
Last edited by: Pegaia at: 24.01.2008 10:55Denilson Pegaia |
|
This contribution was helpful to
1 thankful Users |
Follow us on