11/29/2019 10:55 AM | |
Joined: 12/14/2011 Last visit: 7/24/2025 Posts: 176 Rating:
|
HI to all, i write here the answer from SIEMENS AG Technical Support. This is a known bug: SinaPos instruction cannot be compiled with S7-1200 PLCs in the TIA Portal V15.1 upt to UPD3. There is only the work around at the moment to use the SINA_POS block out from the DriveLib. The DriveLib is (still) installed with Startdrive V15.1. Alternatively you can download it under the link: https://support.industry.siemens.com/cs/ww/en/view/109475044 Many thanks to all. |
This contribution was helpful to
2 thankful Users |
Follow us on