5/3/2020 3:30 PM | |
Posts: 174 Rating: (2) |
what is the fuse rate needed for AI each channel sensor input? Also each DI wire fuse input |
5/19/2020 11:06 AM | |
Joined: 12/10/2018 Last visit: 6/27/2024 Posts: 109 Rating: (11) |
Hello dear Friend Fuse rate for AI Fuse Ratings: Individual channel – Normal 0.5 A Fast blow (Littelfuse P/N: 273.500) (Siemens Spare P/N: A5E01568880) Individual channel – Optional 1.5 A Fast blow (Littelfuse P/N: 273 01.5) (Siemens Spare P/N: A5E01568886) Max total channel current: 8.16 Amps Module NA https://cache.industry.siemens.com/dl/files/986/22091986/att_897946/v1/A5E00482820-012.pdf Fuse rate for DI You can extract the necessary calculations from the attached document Attachmentch3.pdf (352 Downloads) |
Follow us on