6/19/2020 9:54 PM | |
Joined: 9/27/2006 Last visit: 10/2/2024 Posts: 12283 Rating: (2685) |
Hello Addis Ababa; If the unit is straight from the box (litterally), it should work if you respect the system requirements, and the setup procedures. These you will find in the manual for the adapter: https://support.industry.siemens.com/cs/ww/en/view/16983464 The first requirement I would check would be the Windows operating system it was designed to run on. Please see the screenshot below. Hope this helps, |
Follow us on