8/12/2020 12:45 PM | |
Posts: 5 Rating:
|
hello, i have a problem in the same sinamics drive type S120 As when electricity cut out, all machine parameters cleared to ### (somehow over range) and i have to make homing from starter software. and there's one motor attached with mechanical chain, the chain broken every time i make homing as motor moves with its maximum speed to be in reference value please your support to set speed value in homing via starter software instead of moving with maximum speed and also a method to overcome problem of over-range after electric cut out Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/12/2020 13:36:32New subject after splitting |
|
8/17/2020 11:31 AM | |
Posts: 5 Rating:
|
I make save RAM to ROM & save parameters every time using starter on the drive online but once electric fluctuation happens, values cleared to ### |
Follow us on