3/1/2021 10:16 PM | |
Joined: 4/28/2015 Last visit: 3/29/2021 Posts: 4 Rating:
|
Hi, looking for some significant help for a customer project. Recently lost resource supporting node red programming. We use the IoT 2040 with the integrated IO shield. IO Shield # 6ES7647-0KA01-0AA2. I need to program the digital outputs to turn on and off in a defined cycle repetitively with no end. Cycle definitions for each are: DQ(0): On for 24 seconds off for 54 seconds DQ(1): On for 24 seconds off for 276 seconds Is there some on who can create this and send me the .json file I can down load to my device via the SD card? I can offer a STAR award or a beer if we can meet! Please and thank you! User manual for the IO Shield is attached. Can contact me directly @ lawrence.anderson@siemens.com Attachmentiot2000_extension_modules_operating_instructions_enUS_en-US.pdf (316 Downloads) |
3/2/2021 11:01 AM | |
Joined: 4/28/2015 Last visit: 6/3/2024 Posts: 3345 Rating:
|
Hi, please check the attached flow. This was tested with the USER LED and seems to work. The flow always starts with "ON" for 24 seconds after deploying. Guess you owe me a beer ;) Best regards! Attachmentflow_timed_output.txt (316 Downloads) |
Last edited by: bergmanu at: 03/02/2021 11:02:30Not working for IOT2050 support anymore from March 1st, 2024. |
|
3/3/2021 8:52 PM | |
Joined: 4/28/2015 Last visit: 3/29/2021 Posts: 4 Rating:
|
PS - is there a hotline number I can call to get direct support? |
3/4/2021 8:13 AM | |
Joined: 4/28/2015 Last visit: 6/3/2024 Posts: 3345 Rating:
|
Hi, of course this does matter. The MindConnect IoT2040 is a completely different product than the SIMATIC IOT2040. All things we are discussing in this forum are not applicable for the MindConnect IoT2040. For MindConnect IoT2040 support please contact the Technical Support or the MindSphere community. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on