6/10/2017 6:17 AM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating: (77) |
Hi DaveSeda, Compile function will majorly find out whether FB and its IDB are of same version; FC and its call are of same version. Secondly it checks whether correct datatype is connected to all parameters of FB/FC. So update all calls FC. Generate new IDB for FB calls. Note- FBD/LAD/STL editors must be closed while compiling. |
If you like the comment, rate it (right top) or thank it (left bottom). |
|
This contribution was helpful to1 thankful Users |
Follow us on