6/11/2023 3:28 AM | |
Joined: 1/11/2019 Last visit: 11/4/2024 Posts: 790 Rating: (152)
|
Hello, • Hardware: – SIMATIC CPU 41x-5H PN/DP, as of firmware version V6.0 SIMATIC CPU 410-5H (including 410E), as of firmware version V8.2 – IM155-6 PN HA, as of firmware version V1.2 • Software: – S7 F Systems V6.4 (or higher) PCS 7 V9.1 + HUP (or higher) or PCS 7 V9.0 SP3 + HUP (or higher) or – S7 F Systems V6.4 (or higher) STEP 7 V5.6 + SP2 + HF6 (or higher) and CFC V9.0 + SP5 + Upd2 (or higher). Note: Commissioning Make sure that the F capability of the CPU is enabled. The PROFIsafe address must be set or assigned for the F modules. Perform a function test according to your automation task. Only when the correct operation of the safety-related functions is ensured may they be used productively. Note: You can refer the below thread more info |
This contribution was helpful to1 thankful Users |
Follow us on