9/19/2024 8:38 AM | |
Joined: 3/12/2024 Last visit: 8/15/2025 Posts: 183 Rating:
|
Hello edurov, Yes it is possible to install Example Image 1.4 on IOT2050 (Basic/Advanced/M.2/SM). This requires the FW version 1.4. You can download the latest version on our Download Page. If you already using the FW 1.4 then the red status LED indicates an issue with the boot process. Please make sure the Example Image was correctly written on the SD-Card, verify that the SD Card is properly formatted and in good condition and check the boot order. If you still have issues you can also try to connect a serial adapter to get detailed boot messages. Let me know if you need further assistance! BR |
Last edited by: Moderator_Lan at: 09/19/2024 09:08:49link optimized |
|
9/19/2024 11:02 AM | |
Joined: 12/15/2016 Last visit: 6/25/2025 Posts: 77 Rating:
|
The firmware that the IOT has is 1.3.1 I got errors. First it asked me to install python3 progess, I have installed the package. after updating the firmware I get errors. I attach a capture so you can see it. I am installing the firmware by booting the OS from the MMC. I don't understand what the problem is. any idea
AttachmentFoto.zip (420 Downloads) |
Last edited by: edurov at: 09/19/2024 11:03:57 |
|
9/20/2024 12:41 PM | |
Joined: 3/12/2024 Last visit: 8/15/2025 Posts: 183 Rating:
|
Hey edurov, Due to the language I can't identify everything perfect but it looks like there is an error with the BUILD_ID. As python3 is required for the update we recommend you the following steps: 1. Install python3 manually before performing the FW update 2. Use the FW installer tool from IOT2050_Firmware_Update_Files_V1.3.1.zip for the FW update to 1.4 BR |
Last edited by: Moderator_Lan at: 09/20/2024 14:09:12link optimized |
|
3/25/2025 2:43 PM | |
Joined: 7/23/2021 Last visit: 9/10/2025 Posts: 1 Rating:
|
I have same problem also.Pease tell me how to resolve. |
Follow us on