10/10/2016 3:08 PM | |
Joined: 4/28/2015 Last visit: 6/3/2024 Posts: 3345 Rating: (378)
|
You can download the latest SD-Card Example Image here: How the SIMATIC IOT2000 can be put into operation with the SD-Card Example Image please refer to "Setting up the SIMATIC IOT2000". On the download page you can find also the Open Source Software ("OSS") and the Readme-OSS. Hint: This image is valid as of the release hardware of all SIMATIC IOT2020/2040. Tools you will need to operate with the SIMATIC IOT2000:
---------------------17.06.2021--------------------- new features / fixes / improvements in V3.1.1
- updated CIP 4.4 kernel - updated to Node RED 1.2.1 - updated pre-installed nodes - security-fixed Node.js 8.17 - accelerated boot in low-entropy scenarios - improved booting from external media (USB sticks etc.) ---------------------14.07.2020--------------------- new features / fixes / improvements in V2.6.1 - Update to Yocto 2.6 (thud) - Update to nodejs 8 - node-red-contrib-mindconnect, node-red-contrib-iiot-opcua, and node-red-contrib-modbus preinstalled - Prepare over-the-air updates via SWUpdate (requires customized image) - Add timezone configuration support to iot2000setup - workaround for installing node-red-nodes (as with 2.6.0) not required anymore - Various updates and cleanups ---------------------27.06.2019--------------------- new features / fixes / improvements in V2.4.0 - Yocto Rocko (V2.4) - CIP kernel 4.4.154-cip28/-rt20 - Enable peripherals menu on IOT2020 - Fix DHCP in the presence of connman - Enable Realtek RTL8XXX wireless LAN driver - NodeJS v6.14.3 - Added python3-setuptools and python3-lxml - And more!
new features / fixes / improvements in V2.2.0 - Linux Cip Kernel 4.4.105 - Yocto 2.2 (Morty) - Nodejs v6.12.3 - Mosquitto 1.4.14 - Python V2.7.12-r1 - Python3 V3.5.2 - Swap File support (extending RAM) ---------------------19.04.2017--------------------- new features in V2.1.3 - Nodejs v6.9.2 - Mosquitto commandline tools - Pip and python3 modules - File system is expanded at first boot now (please be patient - first boot will last a few minutes due to this) fixes/improvements in V2.1.3 - iot2000setup script improved - node-red issue fixed (starting node-red manually or per autostart will not influence the working directory --> will always be /home/root) ---------------------19.12.2016--------------------- new features in V2.1.2 - npm included in the image - node-red preinstalled - included packages: lsusb, resize2fs, wireless-tools, tree, i2c-tools, sqlite3 - setup script for common tasks (set ip address, hostame etc...) - mraa version 1.5.1 - some firmware files (realtek and broadcom) for usb wifi sticks added - second LED (H6) in IOT2040 is now supported under /sys/class/leds fixes: - load i2c-dev at startup - some parts in the readme were extended - mraa import in python works now |
Last edited by: bergmanu at: 12/19/2016 9:21:04 AMnotes V2.1.2 Last edited by: bergmanu at: 4/19/2017 10:04:31 AMnotes V2.1.3 added Last edited by: bergmanu at: 4/19/2017 10:04:47 AMLast edited by: bergmanu at: 8/9/2017 5:55:55 PMadded links top software Last edited by: bergmanu at: 4/13/2018 1:15:30 PMLast edited by: bergmanu at: 06/27/2019 07:56:02added V2.4 Last edited by: bergmanu at: 04/29/2020 09:13:27changed all IOT2000 to IOT2020/2040 Last edited by: bergmanu at: 05/06/2021 13:05:27added V2.6.1 Last edited by: bergmanu at: 06/17/2021 15:18:52Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to3 thankful Users |
Follow us on