7/23/2013 7:00 AM | |
Posts: 262 Rating:
|
HI,Please refer the attachement to do the online selection of load feeder....For your ease, i am attaching the TYPE 2 for 480V:...1) with Bimettlic relay ( 3RU)3) with 3UF relay ( communication capable)also, like to recommend you new gereration 3RA6 compact starter.FOR 125VDC starter, i suggest you to use DC drives if money is not a contraint.... else you have an option of 3VL MCCBs.Once, you done with your selection of products, please use SERACH BUTTON in the same page above.write the desired MLFB to get the complete datasheet. In contactor, you will find that the coils are capable of 50/60Hz both.
AttachmentAC Starter.zip (1300 Downloads) |
7/23/2013 3:45 PM | |
Posts: 4 Rating:
|
Thns for ur reply Can u send me he control and power diagram for some DC starter panel just for reference?? Thanks |
7/24/2013 7:45 AM | |
Posts: 262 Rating:
|
Hi, You can refer the below link for details of circuit.... however utilization catagories for using AC contactors on DCis also attached herewith. http://www.electrical4u.com/starting-methods-to-limit-starting-current-torque-of-dc-motor/ Hope this will solve your query. Attachment19_06.pdf (1400 Downloads) |
This contribution was helpful to
2 thankful Users |
5/22/2014 4:54 PM | |
Joined: 10/10/2010 Last visit: 7/5/2025 Posts: 309 Rating:
|
DC motor need a DC drive controller in case of speed control or starting and this is diffirent from the AC motor |
5/22/2014 5:31 PM | |
Joined: 1/21/2013 Last visit: 11/20/2024 Posts: 4620 Rating:
|
Hello @nkur Have a look at page 4: Sentron 3VL MCCB Brochure - Hindustan Electric House |
5/22/2014 5:32 PM |
|
Joined: 1/21/2013 Last visit: 11/20/2024 Posts: 4620 Rating:
|
Hello Chetan2490 Havea look at page 4: Sentron 3VL MCCB Brochure - Hindustan Electric House
|
Follow us on