7/12/2007 10:10 AM | |
Posts: 5822 Rating:
|
Hello, if you set all the Functions and Addresses right... I just wonder, do you use the Function PNIO_SEND and PNIO_RECV? Best regards J_Bell |
7/12/2007 10:35 AM | |
Posts: 31 Rating:
|
Here is the project with the network configuration, hope anyone can help me seeng waht im doing wrong.
AttachmentTest_Profinet.zip (728 Downloads) |
7/12/2007 10:35 AM | |
Posts: 31 Rating:
|
And here is the second one. Im using two separated projects for each one of the CPU's, because i need to do that.
AttachmentTest2-Profinet.zip (784 Downloads) |
7/12/2007 11:43 AM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hi I found something, may be?! And continue... See attachments. regards umencho |
7/13/2007 11:12 AM | |
Posts: 31 Rating:
|
Hi, i think now i doing almost everithing right. I have configure the profinet network and the PNIO_SEND and PNIO_RECV in both the IO controler and IO device. But in the IO controler (CP343-1) i keap having the same error in the blocks (8183H). I think this error is related with the adress that im passing to the blocks, but if i change that adress the CPU enters in Sistem Fault, saying that there was an error writing to the P Area. In attachment there is my projects, hoping you can help me. Thank you.
AttachmentProjects.zip (818 Downloads) |
Follow us on