4/5/2023 10:24 AM | |
Joined: 1/24/2021 Last visit: 9/24/2024 Posts: 191 Rating: (21) |
It seems that you want to use angular tool, so you need to create kinematic table for this tool. In attached manual you will find details about this.
Attachmentswiveling (1).pdf (372 Downloads) |
People are divided into those who do Backup and those who will do it. |
|
This contribution was helpful to1 thankful Users |
4/6/2023 5:04 PM | |
Joined: 4/28/2015 Last visit: 9/24/2024 Posts: 45 Rating: (5) |
Have you tried the tool adapter offsets? Tool parameters 21 ... 23: Base dimension / adapter dimension Tool base dimension/adapter dimension can be used when the reference point of the toolholder (tool size) differs from the reference point of the toolholder. This will occur in the following situations:
In order that the discrepancy between the toolholder reference point F and the tool carrier reference point T' can be corrected on the three geometry axes (3-dimensional), all 3 basic lengths are always active irrespective of the tool type. In other words, a twist drill (tool type 200) with a tool length compensation (length 1) can also have a base dimension/adapter dimension in 3 axes. Siemens CNC manuals are available online at https://support.industry.siemens.com/cs/ww/en/view/109801202/145083546763 HTH, SteveA |
Last edited by: Steve_A at: 04/06/2023 17:06:22Last edited by: Steve_A at: 04/06/2023 17:07:42 |
|
This contribution was helpful to1 thankful Users |
5/16/2023 11:27 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Hello community, for the sake of completeness I post the solution from the same topic in the German forum. Translation of the answer from the German topic:
Regards, |
This contribution was helpful to1 thankful Users |
Follow us on