12/6/2017 10:26 AM | |
Posts: 37 Rating: (3) |
Hi HugoD,
When the barcode scanner acts like an USB keyboard, there won't be any ttyUSB device, because keyboards are of the HID USB device class (HID=human input device) and you will find them under /dev/input. ttys have multiple purposes in Linux, one is to use them for communication to a physical device (like the ttyUSB), but they are also used for logical consoles, e.g. the text consoles. Every console has an input and an output device, for local consoles the output is typically the screen and the input is the keyboard. The keyboard is only connected to such a console as long as it has the input focus. When a program like Node-Red is started from an interactive shell, it is attached to the tty of that shell, but normally Node-Red is started as background process without a console. You can change this by starting Node-Red with openvt and assign it directly to a specific console. A pretty good article about ttys can be found here: http://www.linusakesson.net/programming/tty/ You can try is to attach your "barcode keyboard" to one specific (newly created) tty and use this tty from Node-Red. I haven't found the way how to do this, maybe you will find the answer when looking for the following terms: openvt, attach, keyboard, tty, input device. Alternatively you can directly use the input device /dev/input/by-path/* and not a tty, but that is harder because you go one abstraction level deeper. A starting point for the ladder might be these node: https://flows.nodered.org/node/node-red-contrib-autokey https://github.com/MattGyver/node-red-contrib-dev-input The following node will require that Node-Red has the input focus and is not started as background process without any terminal: https://www.npmjs.com/package/node-red-contrib-keypress To use this node assign a tty to Node-Red. This requires the installation of the "kbd" package which contains the openvt tool. Then adapt the/etc/init.d/launch_node-red.sh to look like this:
Using this command should also make it possible to use "/dev/tty" (with no number!) in combination with the serial node. I haven't tested this now, but I used it some years ago with vdr and lirc which had the same problem. Michael |
Last edited by: turner42 at: 12/6/2017 11:17:43 AMLast edited by: turner42 at: 12/6/2017 2:46:53 PMLast edited by: turner42 at: 12/6/2017 2:49:42 PMLast edited by: turner42 at: 12/6/2017 9:20:37 PM |
|
This contribution was helpful to2 thankful Users |
12/6/2017 11:12 PM | |
Posts: 439 Rating: (108) |
Hello Turner42, First of all, thank you very much for the help. I tried to import your flow, but only the "Switch node" is in your export clipboard. The result: I followed your procedure:
Here is what I made:
I suppose you are testing with a UART code reader (right? ), because I can't see anything getting out of the node with a USB keyboard or SIMATIC MV320. I went to the MV320 manual and can't see anything related to UART. USB or RS-232 is the only available communication protocol. There is a RS-232 cable need for RS-232 communication and at this point if I use it I can connect it directly to a PLC module like the COMMUNICATION MODULE CM 1241, RS232.
It's at this point you are using the switch node to connect between output 3 of "exec" node and its input, right? Like that? I added the "#" to the file, but can't get out of my mind you are using a UART reader and me a USB reader. Have a good day! Hugo |
12/8/2017 10:45 PM | |
Posts: 37 Rating: (3) |
Hi HugoD,
As long as the "cat" command is active in Node-Red, you can't access the tty1 from any other command, so you have to stop the flow. Make sure that no other process is using /dev/tty1 using this command:
Normally you would use "fuser" for this purpose, but I think this is not part of the IoT2000 image. The next step is to look, which console has the input focus. On my machine this is tty1, on a normal PC this is a text console on the VGA card. On the IoT2000 it still exists but without VGA/HDMI output you will never see it. Normally you would use "fgconsole" but this is also not part of the IoT2000 image. With the tool "chvt" and using <ALT>-<1> to <8> you could switch the focus between tty1..tty8 (maybe even more), so avoid to press this key combination. Here the output how it looks like when cat is already running in the Node-Red flow:
Now use cat /dev/tty1, enter some characters on the keyboard and press return. Before pressing return, you will see nothing.
I built my image myself and added some of the tools I mentioned. Maybe it is a different version, or different setting. my /proc/tty/drivers and my /sys/class/vtconsole/vtcon0 and kernel cmdline:
I found some interesting documentation about the vts in https://www.kernel.org/doc/Documentation/console/console.txt and https://www.kernel.org/doc/Documentation/fb/fbcon.txt Michael |
Last edited by: turner42 at: 12/8/2017 11:34:44 PMLast edited by: turner42 at: 12/9/2017 12:43:31 PMLast edited by: turner42 at: 12/9/2017 2:35:44 PM |
|
This contribution was helpful to3 thankful Users |
12/12/2017 6:52 PM | |
Posts: 439 Rating: (108) |
Michael, WOW It works! Thank you soooo much! Here is what I did:
You should now see the result in the "Debug" windows. Backspace button also works, this is amazing! Thanks again Michael! Have a good day! Hugo |
Last edited by: HugoD at: 12/12/2017 6:55:00 PM |
|
This contribution was helpful to3 thankful Users |
4/4/2018 1:25 PM | |
Posts: 1 Rating: (0) |
Hello everyone, I'm using a barcode reader from SICK (IDM160-300S), and I've managed to set it up as a USB-serial device and receiving scanned input through Node-red. I believe the same process can be used for any barcode reader that supports to be used as a rs232/serial device over USB. Attached is a couple of images describing the process. Best regards, AttachmentSetup_USB_serial_nodered.zip (697 Downloads) |
This contribution was helpful to1 thankful Users |
3/21/2023 9:36 AM | |
Joined: 6/19/2017 Last visit: 5/24/2024 Posts: 8086 Rating: (165) |
New question published by Arkom P. is split to a separate thread with the subject IOT2050 USB Node-red. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on