6/10/2021 12:55 PM | |
Joined: 1/12/2020 Last visit: 12/26/2022 Posts: 12 Rating: (0) |
Dear Experts, i am facing an issue with synchronization of Redundant S7 414 CPUs. I have uploaded the Program to 01 CPU and its in RUN mode. but other CPU is not going in Run mode. all the synch cables are connected. Both the CPUs rack0 LED glowing green and both are master. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/10/2021 13:46:26New subject after splitting |
|
6/10/2021 12:59 PM | |
Joined: 1/12/2020 Last visit: 12/26/2022 Posts: 12 Rating: (0) |
Dear experts, I have PCS7 V7.0 which is XP based.Can i use same license in PCS7 V9.0. |
Follow us on