(0)| 10/28/2021 7:22 PM | |
|
Posts: 257 Rating:
|
Hello SIOS forum community, We keep receiving questions regarding the replacement battery for the SIMATIC Field PG (programming device) The batteries that could be installed in the SIMATIC Field PG M3: SP303 Order. No. 6ES7798-0AA06-0XA0, SP304 6ES7798-0AA07-0XA0 SP305 Order. No. 6ES7798-0AA08-0XA0 can no longer be ordered as spare parts from Siemens. There are numerous prefabricated offers and solutions regarding replacement batteries for a SIMATIC Field PG M3 on the market. We would be pleased if you share your experiences with the community in this thread. If you have ordered a replacement battery for your Field PG M4, M5 or M6, you will receive the replacement battery Li-Ion 8.25 Ah of the Field PG M6 (Order No. 6ES7798-0AA10-0XA0). For this replacement battery, a BIOS update must be carried out on your Field PG M4 or Field PG M5. Field PG M5 is required. Further information in the following articles: Field PG M3 discontinuation statement Battery SP303 (6ES7798-0AA06-0XA0) was used in the Field PG M3 and has been discontinued since 01.10.2018. Discontinuation declaration Field PG M4 Battery SP304 (6ES7798-0AA07-0XA0) was used in Field PG M4 and has been discontinued since 01.10.2018, substitution type 6ES7798-0AA10-0XA0 Declaration of discontinuation SIMATIC Field PG M5 Battery SP305 (6ES7798-0AA08-0XA0) was used in Field PG M5 and is discontinued since 15.10.2020 Delivery release SIMATIC Field PG M6 Battery SP306 (6ES7798-0AA10-0XA0) is used in the Field PG M6 What has to be considered when transporting a Field PG lithium-ion battery / a complete Field PG? Why is the newly purchased battery not charged in the SIMATIC Field PG? Best regards, SIMATIC International Technical Support Hub |
Follow us on